Axes Group Parameters
Boolean Parameters
This is a list of Boolean parameters currently supported.
These parameters are read and written by the MC_GrpReadBoolPar and MC_GrpWriteBoolPar function blocks A function block groups an algorithm and a set of private data. It has inputs and outputs..
Parameter |
ID |
Name |
R/W |
Description |
---|---|---|---|---|
MC_GRP_PARAM_IGNORE_AXIS_ESTOP |
1000 |
Ignore Axis EStop |
Read/Write |
|
MC_GRP_PARAM_AXIS_ESTOP_ACTIVE |
1001 |
Axis EStop Active |
Read Only |
|
Non-Boolean Parameters
This is a list of non-Boolean parameters currently supported.
These parameters are read and written by the MC_GrpReadParam and MC_GrpWriteParam function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. blocks.
Parameter |
ID |
Name |
R/W |
Description |
---|---|---|---|---|
MC_GRP_PARAM_CIRCLE_TOLERANCE |
2000 |
Read/Write |
|